Configuring the Limits of an Alarm

You configure the limits of an alarm to adjust when an alam triggers or resets.

To configure the limits of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. In the properties pane, click the Alarm Trigger tab.

  3. In the Alarm limit boxes, enter the limits for the alarm.

  4. In the Changes have been made dialog box, click Yes .

  • Alarms Overview
  • Create Out of Range Alarm Wizard – Alarm Trigger Page
  • Create Change of State Alarm Wizard – Alarm Trigger Page
  • Create Multistate Alarm Wizard – Alarm Trigger Page
  • Create Matching Text String Alarm Wizard – Alarm Trigger Page
  • Create Out of Reference Range Alarm Wizard – Alarm Trigger Page
  • Create Sum Alarm Wizard – Alarm Trigger Page
  • Create Enumeration Alarm Wizard – Alarm Trigger Page
  • Create Variable Status Alarm Wizard – Alarm Trigger Page