earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.8, 1.9
4/27/2017

Saving a SmartStruxure Server Device Backup Set to Another Location

You save a backup set from a SmartStruxure server device to another location so you can store the backup set on, for example, a network drive or a USB memory.

To save a SmartStruxure server device backup set to another location
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Backup Sets .

  4. In the List View , open the Local folder for a SmartStruxure server device or the AS Archives folder for an Enterprise Server.

  5. If connected to the Enterprise Server, open the SmartStruxure server device folder that contains the backup set.

  6. Select the backup set that you want to save to a different location.

     
    action_zoom_plus_stroke
  7. On the Actions menu, click Save To .

  8. In the Save As dialog box, enter a storage location and click Save .

  9. Click Close .

     
    action_zoom_plus_stroke
  • Backup Sets
  • Backup Sets View
  • No Restore Files Display After Backup
  • Importing a Backup Set to SmartStruxure Server Device
  • Renamed SmartStruxure Server Device Makes Backup Sets Unavailable