Product version: 3.3, 2022
7/23/2021

Saving an Automation Server Backup Set to Another Location

You save a backup set from an automation server to another location so you can store the backup set on, for example, a network drive or a USB memory.

To save a Automation server backup set to another location
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the EcoStruxure BMS server.

  3. Click Backup Sets .

  4. In the List View , open the Local folder for an automation server or the AS Archives folder for an Enterprise Server.

  5. If connected to the Enterprise Server, open the automation server folder that contains the backup set.

  6. Select the backup set that you want to save to a different location.

  7. On the Actions menu, click Save To .

  8. In the Save As dialog box, enter a storage location and click Save .

  9. Click Close .

  • Backup Sets
  • Control Panel Tab
  • Backup Sets View
  • No Restore Files Display After Backup
  • Importing a Backup Set to Automation Server
  • Renamed Automation Server Makes Backup Sets Unavailable
  • Cannot Save a Backup File using WorkStation