7/12/2022

Creating an Action Note

You create an action note to connect it to an alarm, and to simplify the reporting of actions taken when correcting the problem that triggered the alarm.

Show More
action_close

​Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.

 
action_zoom_plus_stroke Action Notes dialog box

Action Notes dialog box

Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.

​Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To create an action note
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Action notes .

  4. In the A larm Control Panel , in the Action notes view, click the Add action note button

     
    action_zoom_plus_stroke
    .

  5. In the Add Action Note dialog box, in the Name box, type the name of the new action note.

  6. In the Group name box, type a name to create a new group or select an existing group.

  7. In the Description box, type a description for the action note.

  8. Click OK .

  9. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Action Notes View
  • Editing an Action Note
  • Adding an Action Note to an Alarm
  • Configuring Forced User Actions
  • Import and Export of Supporting Objects