You present trend log list values as decimals.
A trend log list displays all values in the trend log in a list.
You can create a trend log list directly from a trend log and refresh the values.
You can manually add records to a trend log list for any type of trend log.
A trend log list can be displayed in a number of ways.
For more information, see Trend Log List Display .
Trend log lists and records can be exported in two different formats:
CSV
XML
For more information, see Export of Trend Log Lists and Records .
Trend log list
In WorkStation, in the System Tree pane, select the trend log list.
On the Trend Log List toolbar, click the Show decimal values button
The values in the trend log list are now shown as decimals.