earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Edit Menu

Use the Edit menu for standard editing of objects.

 
action_zoom_plus_stroke Edit menu

Edit menu

Table: Edit Menu

Command

Description

Search

Click to open Search. For more information, see Search Overview .

Cancel

​Click to cancel the latest command.

Refresh

​​Click to refresh the selected object or workspace.

Select all

Click to select all objects.

Deselect all

Click to deselect all objects.

Cut

​Click to cut the selected objects. The objects are placed on the clipboard.

Copy

​Click to copy the selected objects. The objects are placed on the clipboard.

Paste

​Click to paste a copied or cut object.

Paste as shortcut

Pastes a shortcut to a (copied) folder or object into the selected folder or SmartStruxure server root.

Paste special

Pastes with the all external references intact. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete .

Duplicate

Click to create a configurable number of copies of an object. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete .

Move

Click to move an object to another location. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete .

Delete

​Click to open the Confirm delete dialog box where you delete the selected object. For more information, see Confirm Delete Dialog Box .

Rename

Click to rename the selected object.

Create shortcut

Creates a new shortcut to a selected folder or object into the same folder as the target.

  • WorkStation Toolbar
  • Search Overview
  • Copy, Paste, Duplicate, Move, Rename, and Delete
  • Confirm Delete Dialog Box