earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Editing a Backup Rule

You edit a backup rule on a SmartStruxure server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another SmartStruxure server. 

Show More
action_close

In Building Operation, scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on a SmartStruxure server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

Building Operation automatically backs up all data on a SmartStruxure server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different SmartStruxure servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one SmartStruxure server, which acts as the lead, to manage a recurring backup for a group of SmartStruxure servers. For more information, see Backup Rules View .

To edit a backup rule
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Backup Rules .

  4. Select a backup rule and then click the Edit backup rule button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  5. In the Backup set description box, type or modify the backup comment.

     
    action_zoom_plus_stroke
  6. In the Backup content box, change the type of data you want to back up:

    • Select Configuration only to back up the configuration database and custom object type data. For example, use this option to restore data to a replaced SmartStruxure server with the same name in the system.

    • Select All data to back up the configuration, historical, and custom object type data. For example, use this option to preserve the configuration and historical data for a specified date and time.

  7. In the Lead rule box, enter a backup rule that references a lead schedule managed on another SmartStruxure server.

  8. In the Enabled box, select Yes to enable the backup rule.

  9. Click OK .

  10. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Backup Rules
  • Scheduled Backups
  • Deleting a Backup Rule
  • Editing a Backup Schedule
  • Backup Rules View