earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Schedules
Product version: 3.3, 2022
1/29/2021

Editing a Calendar Exception Event

You edit a calendar exception event to change the information about an exception event.

To edit a calendar exception event
  1. In WorkStation, in the System Tree pane, select the schedule containing the calendar exception event you want to edit.

  2. Click the Basic tab.

  3. In the calendar view, select the date when the calendar exception event you want to edit is valid.

     
    action_zoom_plus_stroke
  4. In the event grid, select the calendar exception event you want to edit. To edit the dates for the calendar exception, you need to separately open the calendar object itself. For more information, see Editing a Date Calendar Event .

  5. Click the Edit schedule event button

     
    action_zoom_plus_stroke
    .

  6. In the Schedule Event Properties dialog box, edit the properties:

    Table: Schedule Event Properties Dialog Box - Calendar Reference View

    Property

    Description

    Event type

    Click Exception to display the exception types.

    Exception type

    Select Calendar to initiate a calendar reference.

    All Day

    Select to create an all day event.

     
    action_zoom_plus_stroke

    Click to add a line to the Times and values box.

     
    action_zoom_plus_stroke

    Click to delete an entry from the Times and values box.

    Name

    Type a name for the event.

    Priority

    Select a priority number between 1 (highest priority) and 16 (lowest priority).

    Calendar

    Select a calendar to reference.

  7. Click OK .

  8. On the File menu, click Save .

  • Exception Events in WorkStation
  • Adding a Calendar Exception Event
  • Schedule Event Properties Dialog Box – Calendar Reference View
  • Editing a Date Calendar Event