earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9
12/14/2016

Editing the Shunt Variables

You add or edit the shunt variables connected to an alarm, to enable or disable the alarm.

To edit the shunt variables
  1. In WorkStation, in the System Tree pane, select the alarm for the shunt variables you want to edit.

  2. Click the Alarm Trigger tab.

  3. Select Invert if you want to invert the shunt variable.

  4. In the Shunt variable 1 box, enter a digital variable that is used as a shunt variable .

     
    action_zoom_plus_stroke
  5. Select an AND or OR operator if you want to add a second shunt variable.

  6. Select Invert to invert the second shunt variable.

  7. In the Shunt variable 2 box, enter a digital variable that is used as a shunt variable .

  8. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Shunt Variables