earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
7/13/2021

Event Archive File

Use the Event Archive to view all events that have passed during the running time of the EcoStruxure BMS server.

 
action_zoom_plus_stroke Event archive file

Event archive file

Table: Event Archive File

Column

Description

TYPE

​Displays the object type that defines the properties of the object.

SEQNO

Displays the trend or event sequence number.

TimeStamp

Displays the date and time when the event was generated.

Description

Displays the description of the object.

EventGUID

Displays the unique identity of the event.

OriginatedGUID

Display the unique identity of the source.

Source

Displays the path of the source object.

SourceServer

Displays the path where the object is located.

Note

Displays the text added to the object in the Note 1 property.

SystemEventId

Displays the event identity generated by the system. For more information, see Event and Alarm Enumerations .

DomainName

Displays the domain the user belongs to.

UserName

Display the name of the user that generated the event.

UniqueUserId

Displays the identity of the user that generated the event.

ValueBefore

Displays the value of an object before it was changed.

ValueAfter

Displays the value of an object after it was changed.

AssignedState

Displays alarms that have been assigned to and accepted by any user or group. For more information, see Event and Alarm Enumerations .

MonitoredVariable

Displays the path of the monitored variable

PreviousAlarmState

Displays the previous alarm state. For more information, see Event and Alarm Enumerations .

AlarmState

Displays the present state of the alarm. For more information, see Event and Alarm Enumerations .

TriggeredTimestamp

Displays the time and date of the last state transfer from normal state to alarm state.

EvaluationState

Displays the present evaluation state of the alarm. For more information, see Event and Alarm Enumerations .

MonitoredValue

Displays the value of the monitored variable.

Priority

​Displays the current priority level of the alarm state.

Count

Displays the number of times the alarm has toggled between the alarm and reset state.

AcknowledgeTime

Displays the time and date when the alarm was acknowledged.

BasicEvaluationState

Displays the alarm state. False represents the alarm is in normal state. For more information, see Event and Alarm Enumerations .

Hidden

Displays False if the object is shown. For more information, see Event and Alarm Enumerations .

Category

Displays the category name of the alarm.

DisabledCause

Displays the cause of the disabled alarm. For more information, see Event and Alarm Enumerations .

ServerOffline

Displays the online status of the EcoStruxure BMS server. For more information, see Event and Alarm Enumerations .

UniqueAlarmId

Displays the unique identity of the alarm.

AlarmText

Displays the alarm messages that are added to the alarm.

Command

Displays the executed command that generated the event.

AssignedToDomain

Displays the domain the user or group that the alarm is assigned to.

AssignedToName

Displays the name of the user or group that the alarm is assigned to.

AssignedToUniqueUserId

​Displays the ID of the user or group that the alarm is assigned to.

GroupName

Displays the name of the cause note or action note that has been edited.

ItemName

Displays the checklist, cause note group, or action note group items that have been edited.

BACnetEventType

Displays the BACnet event. For more information, see Event and Alarm Enumerations .

SystemAlarmId

Displays the alarm ID generated by the system when an alarm is triggered. For more information, see Event and Alarm Enumerations .

Comment

Displays the comment that has been added to an alarm.

  • Event and Alarm Enumerations
  • Archive Log Contents
  • Archiving Overview
  • Manually Creating an Archive
  • Creating a Scheduled Archive