Use the Event View properties for viewing and editing the properties of the Events pane and Event View.
Event View properties
Component |
Description |
Show milliseconds |
Select True to display time properties including milliseconds. |
Number of records shown |
Enter the number of rows you want to list in the Events pane or Event view. You can enter any number between 1 and 5999. |
By default, the latest 1000 event records are displayed in the Event View.
Regardless of the number of event records in the database, you can display a maximum of 5999 event records at a time in the Event View.
You can use the filter to display a different set of event records, maximum 5999 records at a time.