Use the Extended Trend Log properties to configure the extended trend log.
Extended Trend Log properties
Component |
Description |
Monitored trend log |
Enter the trend log that you want to transfer records from. |
Unit |
The unit of an extended trend log created from the trend log wizard at the same time as the connected trend log, inherts the unit of measurement from the connected trend log. The unit of an extended trend log that is manually connected to a trend log, needs to be manually configured to use the same unit of measurement as the connected trend log. |
Smart log |
Select True to optimize the transfer of the monitored trend log to the extended trend log. |
Threshold |
Select the percentage threshold at which the trend log transfers its records to the extended trend log. |
Maximum transfer interva l |
Select the maximum length of time that can pass between transfers from the monitored trend log to the extended trend log. |
Transfer trigger variable |
Enter a trigger variable to force a transfer of all records from the trend log to the extended trend log, for example, to generate a complete report. For more information, see Extended Trend Logs . |
Log size |
Select the number of records to store before old records are overwritten including internal records generated by the trend. |
Include in report s |
Select True to include the extended trend log data in reports. |