earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Server, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Properties Conditions Search

​You can set conditions on object properties that you want to include in the search.

 
action_zoom_plus_stroke ​The Select Conditions dialog box when no object type is selected in the Include types dialog box.

​The Select Conditions dialog box when no object type is selected in the Include types dialog box.

​If you choose to include one or more object types in the search, you can select a condition from the common properties for these object types. If no object type is included in the search, you can select conditions from the general properties for all object types.

If you include only one object in the search you can choose between all the properties for that objects. For example, if you choose Alarm you can select from all alarm properties in the Selection dialog box.

​For example, to search for disabled alarms, you select alarm object type and then select alarm state in the property list.

 
action_zoom_plus_stroke ​The properties available in the Select Conditions dialog box when alarm is selected in the Include types dialog box.

​The properties available in the Select Conditions dialog box when alarm is selected in the Include types dialog box.

​The condition formats looks different depending on property type.

Combining condition groups

You can combine condition groups to better suit your search. The different conditions groups can be combined in any way using "and" and "or".

For example, we want to find all analog values that contain "Setpoint" or "setpoint" in their object names or descriptions. The objects we want to find have a values over 20 or have been modified after 2013-02-25 00:00:00.

A search on these criteria looks like this:

 
action_zoom_plus_stroke You can combine different search criteria in conditions groups to further refine your search.

You can combine different search criteria in conditions groups to further refine your search.

Note:

​Strings in the Select Conditions dialog box are case sensitive, that is they differ between upper and lower case. A description condition for the text string "temperature" is not the same as "Temperature".

  • Search Overview
  • Advanced Search