Use the License Server Address view to specify the address to the License Server.
License Server address view
Component |
Description |
License server address |
Type the address to the License Server where licenses are available for check out. The address must begin with @. To define a port number other than the default port range 27000-27009, type the port number in front of the @, Port-number@Address. Use a semicolon to separate addresses. |