earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: ​License Administrator, ​License Server
Functionalities: License Management
Product version: 1.7, 1.8, 1.9
3/2/2016

Licensing Overview

arrow1_rotationLicense System arrow1_rotationLicense Management arrow1_rotationService and Maintenance

Building Operation is available for all to download and install. However, you need valid licenses to use Building Operation. The number of users of the software is limited to the number of licenses owned by the customer.

License System

​When setting up a new Building Operation system, you need to consider the size of the system, its structure, and the number of licenses to order and distribute.

For more information, see License System .

License Management

A Building Operation license system consists of, for example, a License Server, WorkStation with client tools, and the Enterprise Server. The number of each component varies depending on the system size and architecture.

For more information, see License Management .

Service and Maintenance

The license policy in Building Operation is strictly controlled and is sensitive to any changes on the License Server, both hardware and software.

For more information, see Service and Maintenance .

  • Licensing, Installation, and Localization Overview
  • License System
  • License Management
  • Service and Maintenance