You can only mass create alarms with identical units or no unit. When you mass create trend logs, each trend log gets the same unit as the logged variable.
Objects and properties with no unit are given the unit that is defined for the other objects.