Mass backup is a method of performing a manual, simultaneous backup of all the SmartStruxure servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which SmartStruxure servers you want to back up along with the type of data for each.
In smaller installations, a server group may include an Enterprise Server and one or more SmartStruxure server devices. In larger installations, multiple server groups may include an Enterprise Server with a distinct set of SmartStruxure server devices. In either case, the Enterprise Server is the hierarchical top SmartStruxure server with one or more SmartStruxure server devices.
Mass backup of an Enterprise Server and SmartStruxure server devices
You log on to the Enterprise Server to create a mass backup. For more information, see Backup Options Dialog Box .