earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Object Names

arrow1_rotationMass Rename

All objects in the Building Operation database have to have a name. Building Operation is case-sensitive and differentiates between upper and lowercase characters. ​Two objects cannot have the same name in the same folder even if the objects are of different types.  For example, you cannot create an alarm named Building A and a graphic named Building A in the same folder. However, if you name the graphic Building a, with a lowercase a, you can create it in the same folder as the alarm object Building A.

​The following characters are not allowed in object names in Building Operation.

  • /

  • "

  • ?

  • *

  • ~

  • <

  • >

  • |

  • White space is not allowed in the beginning or the end of an objects name.

  • . (period) is not allowed in the beginning or the end of an objects name.

​There is no limitation of how many characters an object name can have. However, some field devices retain their character limitations when they are added to Building Operation database.

Mass Rename

In WorkStation, you can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.

For more information, see Mass Rename .

  • Building Operation Objects
  • Mass Rename
  • Object Properties
  • Language Packages
  • Regional and Language Overview