Use the Pane properties to configure the settings of the pane.
Pane properties
Component |
Description |
Show toolbar |
Select Yes to show the toolbars for the pane component. |
Default dock position |
Select where to place the pane in the workspace. |
Default visibility |
Select Hidden to hide the pane. |
Dipslay name |
Type the pane name that is to be displayed. Display name is available only in Workstation. |
Initial path |
Enter the path to the pane component. |