Use the Panel properties to configure the properties of a panel.
Panel properties
Component |
Description |
Work area initial path |
Enter the path, for example a graphical link, that points to the panel. |
Show toolbars |
Select Yes to show the toolbars of the panel. |
![]() |
Add Click to add a pane component to the panel. For more information, see Create Object Dialog – Naming the Object Page . |
![]() |
Edit Click to edit a pane component. For more information, see Pane Properties . |
![]() |
Remove Click to remove a panel component. |