Functionalities: User Management
Product version: 3.2, 3.3, 2022
10/15/2020

Predefined Workspaces

​Some workspace layouts are included in the EcoStruxure Building Operation software and cannot be deleted or edited. Those workspaces are located in the local domain of the EcoStruxure BMS server.

Table: Predefined Workspaces

Predefined Workspaces

Description

System Default Workspace

The System Default Workspace displays if there is no workspace available for users that log on to WorkStation. For example, the EcoStruxure Building Operation software uses this workspace when the user account group the user belongs to has no workspaces associated with it, or the user's default workspace is deleted by the system administrator.

Administration Workspace​

The Administration Workspace displays ​if there is no other workspace available for administrators logging on to WorkStation. The purpose of the Administration workspace is to ensure that users with administrator rights always have access to all properties and functions.

Engineering Workspace

​In addition to the System Default Workspace and Administration Workspace that are installed when an EcoStruxure Building Operation software is installed, you also have the option to install a predefined engineering workspace. The purpose of the Engineering workspace is to configure WorkStation, view events and alarms.​

  • Switching Workspaces
  • Selecting a Default Workspace
  • User Account Management Overview
  • Workspace Management