earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.8, 1.9
4/25/2017

Remote Backup and Restore of SmartStruxure Server Devices

When you log on to an Enterprise Server, you can perform remote backups of any SmartStruxure server devices in the system. Whenever a backup occurs on the SmartStruxure server device, the system overwrites the locally stored file on the SmartStruxure server device with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.

When you want to restore a SmartStruxure server device, the system displays only the valid SmartStruxure server device backup files that are stored on the Enterprise Server.

In the event that the backup file on the SmartStruxure server device is damaged or lost, or not the one you want to use, you can select a valid backup file to restore the SmartStruxure server device. The restore operation overwrites the locally stored SmartStruxure server device backup file located on the SmartStruxure server device with the selected backup file. For more information, see Restoring a SmartStruxure Server Device from the Enterprise Server .

  • Manual Backups
  • Backup Sets
  • Restoring a SmartStruxure Server Device from the Enterprise Server