Product version: 3.3, 2022
7/23/2021

Remote Backup and Restore of Automation Servers

When you log on to an Enterprise Server, you can perform remote backups of any automation server in the system. Whenever a backup occurs on the automation server, the system overwrites the locally stored file on the automation server with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.

When you want to restore an automation server, the system displays only the valid automation server backup files that are stored on the Enterprise Server.

In the event that the backup file on the automation server is damaged or lost, or not the one you want to use, you can select a valid backup file to restore the automation server. The restore operation overwrites the locally stored automation server backup file located on the automation server with the selected backup file. For more information, see Restoring an Automation Server from the Enterprise Server .

  • Manual Backups
  • Backup Sets
  • Restoring an Automation Server from the Enterprise Server