Use the Calculated Exception view in the Schedule Event Properties dialog box to schedule recurring exceptions.
Schedule Event Properties dialog box - Calculated exception view
Component |
Description |
Event type |
Click Exception to display the exception types. |
Exception type |
Select Calculated for an exception type to apply to the schedule. |
![]() |
Click to add a line to the Times and values box. |
![]() |
Click to delete an entry from the Times and values box. |
All Day |
Select to create an all day event. |
Name |
Type a name for the event. |
Priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Year |
Displays Any Year which is the default for the calculated exception view. |
Month |
Select a month for the exception event or Odd month , Even month , Any month . |
Week of month |
Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .
|
Week of month |
Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .
|
Day of week |
Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting. |