earth_america
user_standard Log on
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1
10/23/2018

Select Conditions Dialog Box

Use the Select Conditions dialog box to enter property criteria for the object types that are included in the search.

 
action_zoom_plus_stroke Select conditions dialog box with the common properties for all object types.
Figure: Select conditions dialog box with the common properties for all object types.

Table: Select Conditions Dialog Box

Button

Description

Button

Description

 
action_zoom_plus_stroke

Click to add a condition.

 
action_zoom_plus_stroke

Click to remove a condition.

  • Search Overview
  • Search View Toolbar
  • Select Folder Dialog Box
  • Select Types Dialog Box