earth_america
user_standard Log on
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
9/4/2018

Show Hidden Alarms

You show hidden alarms when you want them to be displayed in the Alarms pane or Alarm View.

Show More
action_close

In the Alarms pane or Alarm View, you can hide alarms to decrease the number of alarms and sort out alarms from the list.

A hidden alarm is still active and changes its state as shown alarms. The only difference is that a hidden alarm that goes back to normal state is still visible in the Alarms pane, if hidden alarms are shown.

To show a hidden alarm
  1. In WorkStation, in the Alarms pane or Alarm View, on the Alarm toolbar, click the Show hidden alarms button

     
    action_zoom_plus_stroke
    .

  2. In the Alarms pane, right-click the alarm and then click Show alarm .

The alarm is displayed in the Alarms pane or Alarm View when it is in an alarm state.

  • Hide and Show Alarms
  • Hiding an Alarm
  • Alarms Pane and Alarm View
  • Alarms Pane and Alarm View Toolbar