Use the
Axes
tab to configure the properties of the chart axes.
action_zoom_plus_stroke
Axes tab
Table: Axes Tab
Component
|
Description
|
Time mode
|
Select the time mode of the x-axis.
|
Start time
|
Enter the absolute start time when Time mode is set to
Absolute.
This time is the leftmost point of the x-axis.
|
End time
|
Enter the absolute end time when Time mode is set to
Absolute (start time and end time)
. This time is the rightmost point of the x-axis.
|
Time span
|
Type the relative time span of the x-axis when Time mode is set to
Relative (to current time)
. The rightmost point of the x-axis is the current time.
|
Time zone
|
Select time zone for the trend chart. The time zone is the displayed time perspective of the trend log.
|
Show grid lines
|
Select to show horizontal grid lines.
|
Auto scale left y-axis
|
Select to activate auto scale. The scale of the left Y-axis adapts itself to the displayed series.
|
Left y-axis minimum
|
Type the minimum value of the left y-axis.
|
Left y-axis maximum
|
Type the maximum value of the left y-axis.
|
Show left grid lines
|
Select to show grid lines on the left y-axis.
|
Auto scale right y-axis
|
Select to activate auto scale. The scale of the right y-axis adapts itself to the displayed series.
|
Right y-axis minimum
|
Type the minimum value of the right y-axis.
|
Right y-axis maximum
|
Type the maximum value of the right y-axis.
|
Show right grid lines
|
Select to show grid lines on the right y-axis.
|