Configure the Simple Math Operator properties Basic tab to add, subtract, multiply, or divide one value from another when you perform tests.
Simple math operator
Component |
Description |
Operator |
Select the operator, add, subtract, multiply, or divide. |
In1 |
Input value 1. |
In2 |
Input value 2. |
Value |
Displays the calculated value. |