Use the Status bar to view information on the following items:
connectivity status
security certificates
which EcoStruxure BMS server the user is logged on to
the name of the logged on user account
which domain the user is logged on to
whether or not database mode is active
the current language
the measurement system
Status bar
Component |
Description |
![]() |
Indicates that the security certificate is valid. |
![]() |
Indicates that the security certificate cannot be validated. |
![]() |
Connected to Indicates that WorkStation is connected to the EcoStruxure BMS server. |
![]() |
Trying to connect to Indicates that WorkStation is disconnected from the EcoStruxure BMS server and trying to connect. |
User account |
Displays the account you are currently using. |
Domain |
Displays the domain you are logged on to. |
![]() |
Database mode Indicates that database mode is active. For more information, see Database Mode . |
Current language |
Displays the current display language of the system in the drop-down menu beside the user account. |
Measurement system |
Displays the selected measurement system for the system in the drop-down beside the user account. |