Functionalities: Localization
Product version: 3.2, 3.3, 2022
7/22/2021

Synchronize Time Zone Settings

​​You can establish a lead and shadow relationship to synchronize the time zone settings on all your EcoStruxure BMS servers. The Time Zone object on the lead server contains the time zone settings that are inherited by shadow servers.

This is done automaticallly when you create a new server. For more information, see Creating an Automation Server .

  • Lead and Shadow Relationship
  • Time and Time Zone Configuration in Enterprise Server and Enterprise Central
  • Time and Time Zone Configuration in Automation Server
  • Date & Time View
  • Synchronizing Time Zone Settings on Multiple Automation Servers
  • Creating an Automation Server