Use the Tools menu to open Control Panel or make a number of user settings.
Tools menu
Command |
Description |
Control Panel |
Click to open the Control Panel where you get access to some of the most used administration functions in Building Operation, such as alarms, domains, user accounts, backup and archiving, and engineering. For more information, see Control Panel View . |
Language |
Click to open the Language submenu where you select a different WorkStation language. For more information, see Language Packages . |
Measurement system |
Click to open the Measurement system submenu where you select a different local measurement system. For more information, see Units . |
Options |
Click to open the Options dialog box where you manage some local user settings. For more information, see Options Dialog Box . |