Use the Trend Log Archive to view the history of a trend log.
Trend log archive file
Column |
Description |
TYPE |
Displays the object type that defines the properties of the object. |
SEQNO |
Displays the trend or event sequence number. |
TimeStamp |
Displays the date and time when a record or event was generated. |
RefSeqNo |
Displays a reference to another record by sequence number, used by edits and comments. |
OriginalSeqNo |
Displays the original sequence number from the original log stored by the extended trend log. |
User |
Displays the user that generated the event. |
Comment |
Displays the comment that was added to a record when it was edited. |
Event |
Displays if something is missing or something unexpected happens. For more information, see Trend Log Enumerations . |
EndTime |
Displays the time when the old meter was replaced. |
EndValue |
Displays the value the old meter had when it was replaced. |
StartTime |
Displays the time when the new meter was installed. |
StartValue |
Displays the value of the new meter when it was installed. |
MeterConstant |
Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000. |
MinValue |
Displays the first value of the new meter after roll-over. |
MaxValue |
Displays the last value of the new meter before roll-over. |
Value |
Displays the value of a record. |
EditTime |
Displays the time of the record that is added manually to a manual trend log. |
LogType |
The type of the trend log that has been edited. |
Description |
Displays the trend log property that has been configured. |
Status |
Displays the status of the trend log. For more information, see Trend Log Enumerations . |