earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
5/18/2018

Trend Log Enumerations

An enumeration is a range of values representing a specific command or event. Trend log properties use two enumeration values: Events and Status.

Table: Event

Enumeration value

Enumeration definition

0

Undefined

1

Log started

2

Log stopped

3

Data cleared

4

Log sample missed

5

Config updated

6

Missed upload

7

Time padding

8

Log unconfigured

9

System clock changed

10

Log status

11

Log interrupted

12

Null value

13

Log database restored

14

Log reset by extended log

Table: Status

Enumeration value

Enumeration definition

0

None

1

Offline

2

Forced

4

Invalid

8

Override

16

In alarm

32

Fault

64

Out of service

  • Archive Log Contents
  • Trend Log Archive File