When expanded, the Log Info view displays a summary of the data recorded in the trend log list.
The log info does not include records that are not displayed in the trend log list. The log info data changes with the trend log when the trend log list is refreshed or reopened.
Log info view
Component |
Description |
Log name |
The name of the log that is connected to the trend log list. |
Log unit |
The unit of the recorded values. |
Calculation method |
The calculation method connected to the trend log list, if any. |
Start time |
The time of the first record in the trend log list. |
Highest value |
The highest value in the trend log list. |
Average |
The average value of the trend log list. |
Displayed trend log |
The trend log that is connected to the trend log list. |
Stop time |
The time of the last record in the trend log list. |
Lowest value |
The lowest value in the trend log list. |
Number of records |
The number of records to be stored before old records are overwritten. |