Use the trend log list event icons to get information on different trend log events.
Icon |
Description |
![]() |
Log was started Indicates that the trend log started recording values. |
![]() |
Log was stopped Indicates that the trend log stopped recording values. |
![]() |
The log is not configured Indicates that the trend log is not correctly configured or preferences are missing, so the trend log cannot start recording values. |
![]() |
A log value was missed Indicates that one or more records were missed due to interrupted communication, hardware failure, or software failure. |
![]() |
The log configuration was updated Indicates that the settings of the trend log were updated. The change is described in the comment column of the table. |
![]() |
Record was added Indicates that a record was manually added. |
![]() |
Record was edited Indicates that a record was manually edited. |
![]() |
Record was commented Indicates that a log record was commented. The comment is displayed in the ToolTip of the event and in the comment column of the table. |
![]() |
Log was cleared Indicates that a trend log was cleared. |
![]() |
Meter was changed Indicates that the meter was changed or that the settings were configured. This event symbol only applies to the meter trend log. |
![]() |
System clock changed Indicates that the system date or time, where the trend log is located, has been changed. For more information, see Time and Time Zone . |
![]() |
Override Indicates that the recorded value is overridden by the hardware and is not the measured value. For more information, see Output Override Status . Forced Indicates that the recorded value is forced by the software and is not the measured value. For more information, see Forced I/O Point Values . |
![]() |
Log database restored Indicates that the log database has been restored and that, when the log restarts, there can be a time gap in the log series. |
![]() |
Log reset by extended log Indicates that the commands from the extended trend log have been cleared from the trend log. |