earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, Script Editor, Software Administrator
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Version Numbers and Parallel Installations

The Building Operation version number is constructed with four numbers, which represents different parts of the version: Major, Minor, Maintenance, and Build.

 
action_zoom_plus_stroke Building Operation version number structure
Figure: Building Operation version number structure

Table: Building Operation Version Number Structure

Version number

Description

Major

Increment when major functionality changes are released.

Minor

Increment when minor functionality changes are released.

Maintenance

Increment when correctional changes are released.

Build

A sequential number to guarantee uniqueness of the version release.

When installing a product with a higher version number than what is already installed, the installation package asks you if you want to upgrade or replace your current installation. When starting an installation package with the same version number as the software that is already installed, the installation package asks you whether you want to repair or reinstall the installation.

Notice

Loss of data

Do not execute or run two different versions of a product simultaneously on your server or computer. Running parallel installations can cause data loss or corruption.

Failure to follow these instructions can result in loss of data.

On the same computer or server, you can install products parallel to each other that have different major or minor version numbers. For example, you can install WorkStation 2.1.6.0 on a computer that already has version 1.2.1.0 installed. You have to use different installation folders for parallel versions.

Important:
  • You cannot install parallel License Administrators.

  • You should always run the latest maintenance version of the License Administrator or License Server for your Building Operation version.

Version history log

The version history log contains the following information:

  • The Building Operation versions that have been installed on the computer

  • The hotfix versions that have been installed on the computer

  • The date and time the installation was performed

  • The name of the Windows user account that performed the installation

The version log is created in the installation folder of each Building Operation product. The name of the log file is: version_history.txt .

  • Installation Overview
  • Installation Reparation
  • Reinstallation
  • System Upgrade Overview