Use the View menu to open the Workspaces submenu and to display the System Tree pane, the Alarms pane, and the Events pane.
View menu
Command |
Description |
Workspaces |
Opens the Workspaces submenu where you change workspace. For more information, see View Menu – Workspaces Submenu . |
Alarm View |
Select to display the Alarms pane. For more information, see Alarms Pane and Alarm View . |
Event View |
Select to display the Events pane. For more information, see Alarms Pane and Alarm View . |
System Tree |
Select to display the System Tree pane for the selected SmartStruxure server. For more information, see System Tree Pane . |
Watch |
Select to display the Watch pane. For more information, see Watch Pane in WebStation . |