Use the View menu to display or hide Workspace components.
The View menu
Command |
Description |
Forward |
Click to go forward to a view you have visited before in the selected window. |
Back |
Click to go back to a view you have visited before in the selected window. |
Workspaces |
Use the Workspaces submenu to switch to another workspace. For more information, see View Menu – Workspaces Submenu . |
Save workspace layout |
Click to save workspace layout changes you have made to the workspace on the local computer. For more information, see Workspace Components and Customization . |
Reset workspace layout |
Click to reset workspace layout to the default workspace layout on the local computer. For more information, see Workspace Components and Customization . |
Set the current workspace as default |
Click to set the current workspace layout as the default workspace on the local computer. For more information, see Workspace Components and Customization . |
Toolbars |
Use the Toolbars submenu to hide or display the menus in WorkStation. For more information, see View Menu – Toolbars Submenu . |
Watch |
Select to display the Watch pane where you monitor variables. For more information, see Watch Pane and Watch View . |
System Tree |
Select to display the System Tree where you can see and work with all objects in your system. For more information, see System Tree Pane . |
Events |
Select to display the Events pane where you inspect events. For more information, see Events Pane and Event View Customization . |
Alarms |
Select to display the Alarms pane where you handle alarms. For more information, see Alarms Pane and Alarm View Customization . |
Full screen |
Select to display the selected window in the work area in full screen mode. For more information, see Using Full Screen Mode . |