earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebReports
Functionalities: Reports
Product version: 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Viewing a Prompted Report in WorkStation

You view a prompted report to see a report based on filtering criteria that you enter.

Show More
action_close

A prompted report is a report that processes user-specified filtering criteria to generate the report output. With prompted reports, you enter and select filtering criteria for one or more input parameters, and then run the report. The generated report output provides information that is based on your filtering criteria.

In WebReports, some prompted reports are factory supplied reports provided by Schneider Electric. You receive these reports when you install WebReports, and can view these reports in both WorkStation and your Web browser. For more information, see Factory Supplied Reports .

Other prompted reports are custom reports that you can create using the WebReports features in both WorkStation and your Web browser. For more information, see Custom Reports .

To generate and view a prompted report in WorkStation, you select the report in the Reports folder in the System Tree pane.

 
action_zoom_plus_stroke Prompted Report in the System Tree pane

Prompted Report in the System Tree pane

 
action_zoom_plus_stroke Prompted report output in WorkStation

Prompted report output in WorkStation

When you select the report, the input parameters display in the Work area so you can enter your filtering criteria. After you click Run report, the report output displays in the Work area.

To generate and view a prompted report in your Web browser, you log on to the WebReports Web site, and then select the report in the Reports Tree.

 
action_zoom_plus_stroke Prompted report in the Reports Tree

Prompted report in the Reports Tree

 
action_zoom_plus_stroke Prompted report output in a browser

Prompted report output in a browser

When you select the report, the input parameters display in your browser so you can enter your filtering criteria. After you click Run report, the report output displays in your browser.

To view a prompted report in WorkStation
  1. In WorkStation, in the System Tree pane, expand the folder where the previously saved prompted report resides.

  2. Select the report.

  3. Enter the filtering criteria for the report.

  4. Click Submit Form .

  • Prompted Reports
  • Viewing a Prompted Report in WebReports
  • Creating a Prompted Report in WorkStation
  • Creating a Prompted Report in WebReports