Use the Content tab to edit the content and layout of a workspace.
Content tab
Component |
Description |
Menu |
Select Visible to show the menu in the workspace. |
Address bar |
Select Visible to show the address bar in the workspace. |
Search bar |
Select Visible to show the search bar in the workspace. |
Toolbar |
Select Visible to show the toolbar in the workspace. |
Status bar |
Select Visible to show the status bar in the workspace. |
History bar |
Select Visible to show the history bar in the workspace. |
Root path (Applies to Address Bar and System Tree) |
Displays the path to the basic node of the workspace. For more information, see Workspace Content References . |
![]() |
Add Click to open the Create Object Wizard, where you add a new component to the workspace. For more information, see Create Object Dialog – Naming the Object Page . |
![]() |
Edit Click to edit a pane. For more information, see Pane Properties . |
![]() |
Remove Click to remove a component. |