Product version: 3.3, 2022
7/23/2021

WorkStation

​WorkStation is the interface where you supervise your EcoStruxure BMS. In WorkStation you can also create, modify, and delete objects that are used to build an EcoStruxure BMS.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. For more information, see EcoStruxure Building Operation Software Licensing Installation and Location .

EcoStruxure Building Operation Objects

The EcoStruxure Building Operation database is based on objects. Some objects are created when the database in installed, others are created by the engineer. Depending on the object type and your permissions, you can configure objects in a many different way.

For more information, see EcoStruxure Building Operation Objects .

User Account Management Overview

When logging on to an EcoStruxure BMS server, you have to authenticate yourself by using a valid user account. The user account has to belong to the same domain as the server you log on to.

For more information, see User Account Management Overview .

Workspace Management

The workspace defines the content and layout of WorkStation. The content and layout of the workspace can be adapted different tasks for user accounts or user account groups.

For more information, see Workspace Management .

Database Mode

In WorkStation you use database mode when you want to save configuration changes to the EcoStruxure BMS server database but not send the changes to automation servers or other devices.

For more information, see Database Mode .

  • Products
  • EcoStruxure Building Operation Software Licensing Installation and Location
  • EcoStruxure Building Operation Objects
  • User Account Management Overview
  • Workspace Management
  • Database Mode