Use the Summary tab to edit the basic settings for a user account. For example, you can enable or disable the user account, or change the password for the account.
Summary tab
Component |
Description |
Expires on |
Enter an expiration date and time for the user account. By default, there is no expiration date for the account. |
Disabled |
Select True to disable the user account. |
Force password change |
Select True to force the user to change password after the initial logon. |
Password |
Type the password again. |
Confirm password |
Type the password again. |