earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Localization
Product version: 1.9
12/14/2016

Adding a Language in WebStation

You add a language to WebStation so that the user is able to change to this language.

Important:

To add a language in WebStation, you must log on with a user account that belongs to a user account group that has the property May access device configuration selected in the Policies view.

Note:

When a SmartStruxure server is upgraded, the language pack in WebStation must be added once again. 

Show More
action_close

Building Operation supports several different languages. To be able to install a new language you need a language pack.

Languages in WorkStation

​At the main installation, WorkStation contains English and languages that are avaílable at the time. To support a language, WorkStation needs the specific language package.

You can change the display language from within WorkStation. The changes take effect when you restart WorkStation.

Note:
  • When no language has been actively selected in WorkStation, the language given by the regional settings of the computer's operating system apply provided that the language package for that language is installed.

  • If the language package for the language given by the regional setting is not installed, the WorkStation user interface is displayed in English.

  • In Windows Control Panel , you can check whether or not a language package is installed on the computer.

The language packages are version sensitive, the version of the language package must correspond with the version of WorkStation. If you upgrade your current WorkStation, you must also upgrade your language package version.

WorkStation and servers are built on a multilingual language platform that supports all characters included in the Basic Multilingual Plan, http://unicode.org.

Languages in WebStation

The default language in WebStation is English but this can be changed. The language pack for the language has to be installed on the SmartStruxure server you are connected to using WebStation. Changing the language settings in WebStation only affects the language in your web browser.

The language setting uses session cookies. When you clear the web browser's cache so that the cookie is deleted, you have to change the language once again.

You can change back to the original language or another language if the language pack for the selected language is installed on the server you are connected to.

To be able to install a language pack on the SmartStruxure server, you need the language pack file supplied by Schneider Electric.

To add a language in WebStation
  1. In WebStation, log on to the SmartStruxure server you want to add the language to.

  2. On the main toolbar, on the Settings menu, click Add or remove language .

  3. Click Add .

  4. Browse to the language pack .zip file for the language you want to add.

  5. Click Open .

  6. Click OK.

  • Language Packages
  • Settings Menu
  • Add or Remove Languages Dialog Box
  • Changing the Language in WebStation