Use the Building Operation WebStation window to log on to WebStation.
Building Operation WebStation Widow
Component |
Description |
User name |
Type the user name. |
Password |
Type the password. |
Domain |
Type the name of the domain you want to log on to. If you do not enter a domain, you log on to the EcoStruxure BMS server local domain. For more information, see Domains . |
Log on |
Click to log on to WebStation. |
Log on as guest |
Click to log on as guest. This button is only available if a guest account is configured. For more information, see Guest User Account . |
Log on with SSO |
Click to log on with SSO. This button is only available if a SSO is available using Federated Authentication. For more information, see Federated Authentication . |
Click here to learn more about Building Operation |
Click to open the WebHelp home page. For more information, see WebHelp Overview . |