Functionalities: Trends
Product version: 3.2, 3.3, 2022
10/15/2020

Editing an Extended Trend Log to be Included in Reports

You edit extended trend logs to be included in reports if you want trend log data to appear in the reports.

To edit an extended trend log to be included in reports
  1. In WorkStation, in the System Tree pane, click the extended trend log you want to include in reports.

  2. In the Extended Trend Log properties, in the Include in Reports box, select True .

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

The extended trend log is set up to be included in reports.

  • Configuring an Extended Trend Log
  • Extended Trend Log Properties – Basic Tab
  • Extended Trend Logs