earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
User Interface

User Interface


Products: WebReports
Functionalities: Reports
Product version: 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Electricity Meter Properties – Basic Tab

Use the ​ Basic tab to enter meter numbers, associate the meter with an extended trend log, and to add or remove tags.

 
action_zoom_plus_stroke Basic tab

Basic tab

Table: Basic Tab

Property

Description

Utility

Displays the utility selected on creation of the meter.

Meter Reference Number

Type the meter reference number.

Meter Serial Number

Type the meter serial number.

Meter Trend Log

Enter the path of the extended trend log you want to associate with this meter.

Attached tags

Displays all tags attached to the energy object.

Enter a new tag

Type the text you want to be displayed in a new tag.

 
action_zoom_plus_stroke

Click to place a new tag in the Attached tags area after you have entered text in the Enter a new tag box.

 
action_zoom_plus_stroke

Click to open the Add Existing Tags dialog box. For more information, see Add Existing Tags Dialog Box .

  • General Information Properties – Basic Tab
  • Energy Monitoring Reports
  • Energy Object Tagging
  • Attaching a New Tag to an Energy Object
  • Add Existing Tags Dialog Box