earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Alarms
Product version: 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
1/25/2018

Adding and Removing Columns in Alarm View and Event View

You add or remove columns to get a better overview of the properies in the Alarm View and Event View.

Show More
action_close

You can customize the columns in an Alarm View and an Event View to make it easier to get an overview over the properties that are displayed in the view.

You can add or remove columns. When you log off from WebStation or refresh the browser the Alarm View and Event View returns to the default columns.

 
action_zoom_plus_stroke Alarms View with default columns (top) and customized with the columns for State, Source, Alarm text, Triggered time, Acknowledged by, and Category (bottom).

Alarms View with default columns (top) and customized with the columns for State, Source, Alarm text, Triggered time, Acknowledged by, and Category (bottom).

To add and remove columns in Alarm View and Event View
  1. In WebStation, in the Alarm view or Event view, right-click the column head and then click Add/remove columns .

  2. In the Add/Remove dialog box, select the columns you want to add.

  3. Click Close .

When you log out from WebStation or refresh the Web browser the Alarm View and Event View return to the default columns.

  • Alarm and Event View Columns Customization in WebStation
  • Alarms Pane and Alarm View
  • Events Pane and Event View
  • Add/Remove Columns Dialog Box