Use the Initial Meter Settings page to set the initial values for the meter trend log.
Initial meter settings page
Property |
Description |
Start time |
Displays the time when the new meter was installed. |
Start value |
Displays the value of the new meter when it was installed. |
Min value |
Displays the first value of the new meter after roll-over. |
Max value |
Displays the last value of the new meter before roll-over. |