Functionalities: User Management
Product version: 3.2, 3.3, 2022
10/15/2020

Command Permissions

arrow1_rotationCommand Permissions Rules

Command permissions are used to control the operations the members of a user account group can perform on a category of objects in the EcoStruxure Building Operation database. You use command permissions to configure exceptions from path permissions.

Command Permissions Rules

You use command permissions to configure exceptions from path permissions. You can set the following permissions for a command: no setting, deny, allow.

For more information, see Command Permissions Rules .

  • Software Permissions
  • Command Permissions Rules