earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Server, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Archive Settings Manager Dialog Box

Use the Archive Settings Manager to archive events and extended and trend logs on the Enterprise Server.

 
action_zoom_plus_stroke Archive Settings Manager dialog box

Archive Settings Manager dialog box

Table: Archive Settings Manager Dialog Box

Number

Description

Enabled

Select to activate the archiving function on the Enterprise Server. For more information, see Enabling the Archiving Function and Defining the Archive Folder .

Disabled

Select to disable the archiving function on the Enterprise Server.

Archive Now

Click to archive the selected historical data immediately. For more information, see Manually Creating an Archive .

Alarm Events

Select to include Alarm events in the archive.

User Events

Select to include User events in the archive.

System Events

Select to include System events in the archive.

Add extended trend log icon

Click the plus sign

 
action_zoom_plus_stroke
to add an extended trend log to the list.

Remove extended trend log icon

Click the remove sign

 
action_zoom_plus_stroke
to delete an extended trend log to the list.

Extended Trend Log

Select the logs that you want to include in the archive.

Archive Schedule

Click Schedule to configure a schedule for archiving. For more information, see Manual and Scheduled Archiving .

Output Type

Select an output type for the archive. For more information, see Archiving Formats and Storage .

Path

Type the path to the location where you want store the archive files. For more information, see Enabling the Archiving Function and Defining the Archive Folder .

Validate

Click to validate that the path is valid. A green checkmark

 
action_zoom_plus_stroke
displays if the system successfully validates the path.

  • Enabling the Archiving Function and Defining the Archive Folder
  • Creating a Scheduled Archive
  • Manually Creating an Archive
  • Manual and Scheduled Archiving
  • Archiving Formats and Storage